Channel Bonding Temperature Compensation Using SCPI

Other Keysight Technologies signal generators provided the ability to apply temperature compensation, which adjusted the phase relationship between the two channels to better maintain the phase relationship between the two channels at the carrier frequency. The Temperature Compensation SCPI commands are provided to allow programmatic compatibility with those instruments.

Enable Periodic Temperature Compensation

Temperature Compensation Cycle Time

Temperature Compensation Averaging

Immediate Temperature Compensation

Temperature Compensation Coefficient

Measured Bonded Temperature

Measured Periodic Temperature

Immediate Measured Temperature

Enable Periodic Temperature Compensation

Remote Command only

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce]:GROup<group>:CBONded:TCOMpensate[:STATe] ON|OFF|1|0

[:SOURce]:GROup<group>:CBONded:TCOMpensate[:STATe]?

SCPI Example

GRO:CBON:TCOM OFF

Preset

ON

Notes

This command is accepted and does not raise an error.

State Saved

Yes

Initial S/W Revision

A.10.00

Temperature Compensation Cycle Time

Remote Command only

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce]:GROup<group>:CBONded:TCOMpensate:CTIMe <integer>

[:SOURce]:GROup<group>:CBONded:TCOMpensate:CTIMe?

SCPI Example

GRO:CBON:TCOM:CTIM 5

Preset

10

Notes

This command is accepted and does not raise an error.

State Saved

Yes

Min

1

Max

3600

Resolution

1 (seconds)

Initial S/W Revision

A.10.00

Temperature Compensation Averaging

Remote Command only

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce]:GROup<group>:CBONded:TCOMpensate:TAVeraging <integer>

[:SOURce]:GROup<group>:CBONded:TCOMpensate:TAVeraging?

SCPI Example

GRO:CBON:TCOM:TAV 20

Preset

10

Notes

This command is accepted and does not raise an error.

State Saved

Yes

Min

0

Max

100

Resolution

1

Initial S/W Revision

A.10.00

Immediate Temperature Compensation

Remote Command only

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce]:GROup<group>:CBONded:TCOMpensate:IMMediate

SCPI Example

GRO:CBON:TCOM:IMM

Preset

N/A

State Saved

N/A

Notes

This command performs no action and does not raise an error.

Initial S/W Revision

A.10.00

Temperature Compensation Coefficient

Remote Command only

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce]:GROup<group>:CBONded:TCOMpensate:COEFficient <real>

[:SOURce]:GROup<group>:CBONded:TCOMpensate:COEFficient?

SCPI Example

GRO:CBON:TCOM:COEF 33.0

Preset

30.0

State Saved

Yes

Min

25.0

Max

35.0

Resolution

0.001

Notes

This command is accepted and does not raise an error.

Initial S/W Revision

A.10.00

Measured Bonded Temperature

Remote Command only

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce]:GROup<group>:CBONded:TCOMpensate:TBONded?

SCPI Example

GRO:CBON:TCOM:TBON?

Units

Degrees Celsius

Preset

0.0

State Saved

Yes

Resolution

0.1

Notes

This command is accepted and returns the preset value.

Initial S/W Revision

A.10.00

Measured Periodic Temperature

Remote Command only

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce]:GROup<group>:CBONded:TCOMpensate:TPERiodic?

SCPI Example

GRO:CBON:TCOM:TPER?

Units

Degrees Celsius

Preset

0.0

State Saved

Yes

Resolution

0.1

Notes

This command is accepted and returns the preset value.

Initial S/W Revision

A.10.00

Immediate Measured Temperature

Remote Command only

Provided to allow programmatic compatibility with other Keysight Technologies signal generators. Command is accepted but does nothing.

SCPI Command

[:SOURce]:GROup<group>:CBONded:TCOMpensate:TIMMediate?

SCPI Example

GRO:CBON:TCOM:TIMM?

Units

Degrees Celsius

Preset

0.0

State Saved

Yes

Resolution

0.1

Notes

This command is accepted and returns the preset value.

Initial S/W Revision

A.10.00